Everything
2.11.6.2 Putting the registered watch-expressions in order

The registered watch-expressions can be classified by a category (folder) for display in tree form (By default, there are no categories.).

Caution 1.

No other categories can be created within a category.

Caution 2.

Up to 64 categories can be created in one Watch panel. (If an attempt is made to create beyond the upper limit, a message is displayed.).

(1)

To create a new category

Move the caret to the position at which you want to create and then click the toolbar button and enter a new category name directly from the keyboard.

(2)

To edit a category name

Select a category name you want to edit and then click on it again and edit the category name directly from the keyboard.

(3)

To remove a category

Select a category you want to remove and then click the toolbar button .

(4)

To change the order in which watch-expressions are displayed

Drag-and-drop a registered watch-expression directly onto the category you've created. That way, watch-expressions are classified by a category.

Also, the order in which categories and watch-expressions are displayed (one above or below another) can be freely changed by a drag-and-drop operation.

Remark

If categories or watch-expressions in a watch panel are drag-and-dropped into another Watch panel (Watch1 to Watch4), the categories or watch-expressions are copied into the target Watch panel.