Everything

csplus.remove_event_listener


This function removes the specified listener from the list of functions to be called when an event happen in CS+.

[Specification format]

csplus.remove_event_listener(listener)

[Argument(s)]

Parameter

Description

listener

Specifies the listener function to remove.

[Return value]

None

[Example of use]

>>> def listener1(event): print("Listener 1: " + event)
...
>>> csplus.add_event_listener(listener1)
>>> csplus.remove_event_listener(listener1)
>>>