Everything

csplus.add_address_breakpoint


This command adds an address breakpoint with additional type setting.

[Specification format]

csplus.add_address_breakpoint(address, breakpoint_type="", temporary=False)

[Argument(s)]

Argument

Description

address

The address to set breakpoint at

breakpoint_type

The type of breakpoint to be set, either "Hardware" or "Software" (case-insensitive).

If not inputted or inputted with other value, the type will be decided by CS+.

temporary

A flag indicating whether the breakpoint should be hit only once or not

[Return value]

The index of the added breakpoint in the list of all breakpoints

[Detailed description]

-

The returned value is just the index at the time the breakpoint is added. It may be changed when other breakpoints are added/removed.

[Example of use]

>>> csplus.add_address_breakpoint(0x12, "hardware", True)
2