Everything

csplus.set_integer_expression


This function sets value of a integer expression.

[Specification format]

csplus.set_integer_expression(session_id, expression, value)

[Argument(s)]

Argument

Description

session_id

This argument is ignored in this version.

expression

The expression to be evaluated

value

The integer value to set to the specified expression

[Return value]

None

[Detailed description]

-

This function sets value of a integer expression.

[Example of use]

>>> csplus.set_integer_expression(0, "intVar", 10)
>>> csplus.get_integer_expression(0, "intVar")
10