Everything
2.10 Save the Project File

Information on the settings for a project is saved in the project file (*.mtpj) and the environment-dependent information-saving file (*.mtud).

Select the [File] or [Project] menu >> [Save Project].

When there is a change in the project, the message dialog box below will open.

Figure 2.97

Message Dialog Box

 

To continue with the operation, click the [Yes] button on the dialog box.

The project file is overwritten with the current settings information.