2.5.2 Set a macro definition

Select the build tool node on the project tree and select the [Assemble Options] tab on the Property panel.

The macro definition setting is made with the [Macro definition] property in the [Source] category.

Figure 2.32

[Macro definition] Property

 

If you click the [...] button, the Text Edit dialog box will open.

Figure 2.33

Text Edit Dialog Box

 

Enter the macro definition in the format of "macro name=string", with one macro name per line.

You can specify up to 32767 characters per line, up to 65535 line.

If you click the [OK] button, the entered macro definitions are displayed as subproperties.

Figure 2.34

[Macro definition] Property (After Setting Macros)

 

To change the macro definitions, you can use the [...] button or enter the path directly in the text box of the subproperty.

Remark

You can also set the option in the same way with the [Macro definition] property in the [Frequently Used Options(for Assemble)] category on the [Common Options] tab.