This panel is used to display the detailed information on the Build tool node or file that is selected on the Project Tree panel by every category and change the settings of the information.
The following items are explained here.
On the Project Tree panel, select the Build tool node or file and then select [Property] from the [View] menu or [Property] from the context menu. |
When either one of the Build tool node or file on the Project Tree panel is selected while the Property panel has been opened, the detailed information of the selected item is displayed. |
In this area, the detailed information on the Build tool node or file that is selected on the Project Tree panel is displayed by every category in the list. And the settings of the information can be changed directly.
Mark
indicates that all the items in the category are expanded. Mark
indicates that all the items are collapsed. You can expand/collapse the items by clicking these marks or double clicking the category name.
Mark
indicates that only a hexadecimal number is allowed to input in the text box.
See the section on each tab for the details of the display/setting in the category and its contents.
Categories for the display of the detailed information are changed by selecting a tab.
In this panel, the following tabs are contained (see the section on each tab for the details of the display/setting on the tab).
When multiple components are selected on the Project Tree panel, only the tab that is common to all the components is displayed. |
[Build Settings] tab (for C source file, assembly source file, object file, and library file) |
[Individual Compile Options(C)] tab (for C source file) |
[Individual Compile Options(C++)] tab (for C++ source file) |
[Individual Assemble Options] tab (for assembly source file) |
See "CS+ Integrated Development Environment Users Manual: Project Operation" for details about the [File Information] tab. |
[[Edit] menu (only available for the Property panel)]
|
Cancels the previous edit operation of the value of the property. |
|
|
While editing the value of the property, cuts the selected characters and copies them to the clipboard. |
|
|
Copies the selected characters of the property to the clipboard. |
|
|
While editing the value of the property, inserts the contents of the clipboard. |
|
|
While editing the value of the property, deletes the selected characters. |
|
|
While editing the value of the property, selects all the characters of the selected property. |
|
|
Restores the configuration of the selected item to the default configuration of the project. For the [Individual Compile Options(C)] tab, [Individual Compile Options(C++)] tab, and [Individual Assemble Options] tab, restores to the configuration of the general option. |
|
|
Restores all the configuration of the current tab to the default configuration of the project. For the [Individual Compile Options(C)] tab, [Individual Compile Options(C++)] tab, and [Individual Assemble Options] tab, restores to the configuration of the general option. |