Renesas Electronics
R_IT8bitm_Channeln_Create
Performs initialization necessary to control the 8-bit interval timer.
[Syntax]
void R_IT8bitm_Channeln_Create ( void );
Remark
m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]