Renesas Electronics
Below is a list of API functions output by the Code Generator for 8-bit interval timer use.
Table 3.16
API Functions: [8-Bit Interval Timer]
API Function Name
Function
R_IT8bitm_Channeln_Create
Performs initialization necessary to control the 8-bit interval timer.
R_IT8bitm_Channeln_Create_UserInit
Performs user-defined initialization relating to the 8-bit interval timer.
r_it8bitm_channeln_interrupt
Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1.
R_IT8bitm_Channeln_Start
Starts the count of the 8-bit interval timer.
R_IT8bitm_Channeln_Stop
Ends the count of the 8-bit interval timer.
R_IT8bitm_Channeln_Set_PowerOff
Halts the clock supplied to the 8-bit interval timer.