R_IT8bitm_Channeln_Stop


Ends the count of the 8-bit interval timer.

[Syntax]

void    R_IT8bitm_Channeln_Stop ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.