3.3 Link Map File (When Objects Are Combined)

This section explains the link map file that is output when the object combine function is used in a multi-core project.

The link map file has detailed information regarding object combining.