Renesas Electronics
The version information and the time of linkage are output.
The output example of the header information is shown below.
Renesas Optimizing Linker (VX.XX.XX) XX-Xxx-XXXX XX:XX:XX (1)
Number
Description
(1)
Version information of the optimizing linker and time of linkage
The version information of the optimizing linker and the time of linkage are output.