3.3.6  
Combined address information
 
The combined source files, and the start and end addresses and size of the continuous range data are output.
The output example of the combined address information is shown below.
*** Combine information *** 
(1)             (2)         (3)         (4) 
FILE            START       END         SIZE 
sample1.mot 
                00000100    00000127    28 
sample1.mot 
                00000200    00000227    28 
sample2.mot 
                00000250    00000263    14 
sample2.mot 
                00000300    0000033b    3c 
 | 
 
| 
 | 
 | 
| 
 | 
 
Combined source file name 
The combined source file name is output. 
 | 
| 
 | 
 
Start addresses of continuous range data 
The start addresses of the continuous range data are output. 
This is expressed in a hexadecimal number. 
 | 
| 
 | 
 
End addresses of continuous range data 
The end addresses of the continuous range data are output. 
This is expressed in a hexadecimal number. 
 | 
| 
 | 
 
Size of continuous range data 
The size of the continuous range data is output (in byte units). 
This is expressed in a hexadecimal number. 
 |