This option outputs debug information to the output file.
The debug information is output to the output file (It is the same result as when the -debug option is specified).
If the -form={object|library|hexadecimal|stype|binary}, -strip option or -extract option is specified, this option will be invalid. |
If two or more output file names are specified using the -form=absolute option and -output option, the debug information will not be output. |