This option does not output the debug information.
[Specification format]
 
-  | Interpretation when omitted  | 
 
The debug information is output to the output file (It is the same result as when the -debug option is specified).
[Detailed description]
-  | This option does not output the debug information.  | 
 
[Example of use]
-  | Not to output the debug information, describe as:  | 
 
>rlink a.obj b.obj -nodebug -output=c.abs 
 | 
 
[Remark]
-  | If the -form={object|library|hexadecimal|stype|binary}, -strip option or -extract option is specified, this option will be invalid.  |