This option stores address values in the specified areas in the vector table.
[Specification format]
-VECTN=[vector-number={symbol|address}][,vector-number={symbol|address}]...
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option stores the specified address values in the specified locations of the vector table. |
- | When this option is specified, the optimizing linker creates a vector table section and stores the specified address values in the vector table even if no interrupt handlers are written in the source program. |
- | Specify a hexadecimal value from 0 to 255 as vector-number. |
- | Specify the external name of the target function prefixed with an underscore (_) as symbol. |
- | Specify the desired hexadecimal address for address. |
- | The value to be set at address 0x2 and 0x3 of the vector table is determined in the following order of priority.
-rrm option > -debug_monitor option > Assembly source file specification > -vectn option > -vect option
|
[Example of use]
- | To store the address of _dummy at address 0x14 in the vector table, describe as: |
>rlink a.obj b.obj -vectn=14=_dummy
|
[Remark]
- | This option is ignored when the user creates a vector table address section in the source program because the vector table is not automatically created in this case. |
- | If the -form={object|relocate|library} option, -strip option, or -extract option is specified, this option will be invalid. |