< Compile Options / Optimize Options >
When the speed option is specified, optimization will be performed with emphasis on execution performance. |
When the speed option is specified, the following options are automatically specified based on the optimize option specification. |
The default is map when a C/C++ source program has been specified for input and output=abs or output=mot has been specified for output. For any other case, the default is nomap. |