< Compile Options / Optimize Options >
[Format]
[Description]
- | When the size option is specified, optimization will be performed with emphasis on code size. |
[Remarks]
- | When the size option is specified, the following options are automatically specified based on the optimize option specification. Note however that if one of the following options is specified otherwise explicitly, that specified option becomes valid. |
- | When optimize=max is specified |
|
|
|
|
|
|
|
|
|
|
|
size
|
loop=1
|
inline=0
|
noconst_div
|
schedule
|
const_
copy
|
noscope
|
map*
nomap*
|
alias=ansi
|
Note | The default is map when a C/C++ source program has been specified for input and output=abs or output=mot has been specified for output. For any other case, the default is nomap. |
- | When optimize=2 is specified |
|
|
|
|
|
|
|
|
|
|
|
size
|
loop=1
|
noinline
|
noconst_div
|
schedule
|
const_
copy
|
scope
|
nomap
|
alias=noansi
|
- | When optimize=0 or optimize=1 is specified |
|
|
|
|
|
|
|
|
|
|
|
size
|
loop=1
|
noinline
|
noconst_div
|
noschedule
|
noconst_
copy
|
scope
|
nomap
|
alias=noansi
|