< Compile Options / Microcontroller Options >
[Format]
The default for this option is endian=little.
[Description]
- | When endian=big is specified, data bytes are arranged in big endian. |
- | When endian=little is specified, data bytes are arranged in little endian. |
- | The endian type can also be specified by the #pragma endian extension. If both this option and a #pragma extension are specified, the #pragma specification takes priority. |