< Compile Options / Microcontroller Options >
When this option is omitted, it does not generate the saved and restored code of the accumulator (ACC,ACC0,ACC1) for interrupt functions.
This option generates the saved and restored code of the accumulator (ACC,ACC0,ACC1) for interrupt functions. |
The save and restored code of the ACC when the ISA *1 is selected as the RXv1 or the microcomputer type is selected by the CPU *2. |
*1) This means a selection by the -isa option or the ISA_RX environment variable.
*2) This means a selection by the -cpu option or the CPU_RX environment variable.