5.1.3 Coding of Labels

Be sure to append a colon (:) to the end of a label.

Example

LABEL1:

Defining a symbol name which is the same as that of an existing section is not possible. If a section and symbol with the same name are defined, the section name will be effective, but the symbol name will lead to an A2118 error.