5.1.8
Selection of Optimum Instruction Format
Some of the RX Family microcontroller instructions provide multiple instruction formats for an identical single processing.
The assembler selects the optimum instruction format that generates the shortest code according to the instruction and addressing mode specifications.
For an instruction having an immediate value as an operand, the assembler selects the optimum one of the available addressing modes according to the range of the immediate value specified as the operand. The following shows the immediate value ranges in the order of priority.
Table 5.12 | Ranges of Immediate Values |
|
|
|
|
|
#imm:1
|
1 to 2
|
1H to 2H
|
|
#imm:2
|
0 to 3
|
0H to 3H
|
|
#imm:3
|
0 to 7
|
0H to 7H
|
|
#imm:4
|
0 to 15
|
0H to 0FH
|
|
#imm:5
|
0 to 31
|
0H to 1FH
|
|
#imm:8
|
128 to 255
|
80H to 0FFH
|
|
#uimm:8
|
0 to 255
|
0H to 0FFH
|
|
#simm:8
|
128 to 127
|
80H to 7FH
|
|
#imm:16
|
32768 to 65535
|
8000H to 0FFFFH
|
|
#simm:16
|
32768 to 32767
|
8000H to 7FFFH
|
|
#simm:24
|
8388608 to 8388607
|
800000H to 7FFFFFH
|
|
#imm:32
|
2147483648 to 4294967295
|
80000000H to 0FFFFFFFFH
|
Notes 1. | Hexadecimal values can also be written in 32 bits.
Example: Decimal "127" = hexadecimal "7FH" can be written as "0FFFFFF81H". |
Notes 2. | The #imm range for src in the INT instruction is 0 to 255. |
Notes 3. | The #imm range for src in the RTSD instruction is four times the #uimm:8 range. |
(2) | ADC and SBB Instructions |
The following shows the ADC and SBB instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Note | The following table does not show the instruction formats and operands for which code selection is not optimized. When the processing size is not shown in the table, L is assumed. |
Table 5.13 | Instruction Formats of ADC and SBB Instructions |
|
|
|
|
|
|
|
|
|
ADC src,dest
|
#simm:8
|
|
Rd
|
4
|
|
#simm:16
|
|
Rd
|
5
|
|
#simm:24
|
|
Rd
|
6
|
|
#imm:32
|
|
Rd
|
7
|
|
ADC/SBB src,dest
|
dsp:8[Rs].L
|
|
Rd
|
4
|
|
dsp:16[Rs].L
|
|
Rd
|
5
|
|
|
|
|
|
|
In the SBB instruction, an immediate value is not allowed for src.
The following shows the ADD instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.14 | Instruction Formats of ADD Instruction |
|
|
|
|
|
|
|
|
|
(1) ADD src,dest
|
#uimm:4
|
|
Rd
|
2
|
|
#simm:8
|
|
Rd
|
3
|
|
#simm:16
|
|
Rd
|
4
|
|
#simm:24
|
|
Rd
|
5
|
|
#imm:32
|
|
Rd
|
6
|
|
dsp:8[Rs].memex
|
|
Rd
|
3 (memex = UB), 4 (memex UB)
|
|
dsp:16[Rs].memex
|
|
Rd
|
4 (memex = UB), 5 (memex UB)
|
|
(2) ADD src,src2,dest
|
#simm:8
|
Rs
|
Rd
|
3
|
|
#simm:16
|
Rs
|
Rd
|
4
|
|
#simm:24
|
Rs
|
Rd
|
5
|
|
#imm:32
|
Rs
|
Rd
|
6
|
(4) | AND, OR, SUB, and MUL Instructions |
The following shows the AND, OR, SUB, and MUL instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.15 | Instruction Formats of AND, OR, SUB, and MUL Instructions |
|
|
|
|
|
|
|
|
|
AND/OR/SUB/MUL
src,dest
|
#uimm:4
|
|
Rd
|
2
|
|
#simm:8
|
|
Rd
|
3
|
|
#simm:16
|
|
Rd
|
4
|
|
#simm:24
|
|
Rd
|
5
|
|
#imm:32
|
|
Rd
|
6
|
|
dsp:8[Rs].memex
|
|
Rd
|
3 (memex = UB), 4 (memex UB)
|
|
dsp:16[Rs].memex
|
|
Rd
|
4 (memex = UB), 5 (memex UB)
|
In the SUB instruction, #simm:8/16/24 and #imm:32 are not allowed for src.
The following shows the BMCnd instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.16 | Instruction Formats of BMCnd Instruction |
|
|
|
|
|
|
|
|
|
|
BMCnd src,dest
|
B
|
#imm:3
|
|
dsp:8[Rs].B
|
4
|
|
B
|
#imm:3
|
|
dsp:16[Rs].B
|
5
|
The following shows the CMP instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.17 | Instruction Formats of CMP Instruction |
|
|
|
|
|
|
|
|
|
|
CMP src,src2
|
L
|
#uimm:4
|
Rd
|
|
2
|
|
L
|
#uimm:8
|
Rd
|
|
3
|
|
L
|
#simm:8
|
Rd
|
|
3
|
|
L
|
#simm:16
|
Rd
|
|
4
|
|
L
|
#simm:24
|
Rd
|
|
5
|
|
L
|
#imm:32
|
Rd
|
|
6
|
|
L
|
dsp:8[Rs].memex
|
Rd
|
|
3 (memex = UB),
4 (memex UB)
|
|
L
|
dsp:16[Rs].memex
|
Rd
|
|
4 (memex = UB),
5 (memex UB)
|
(7) | DIV, DIVU, EMUL, EMULU, ITOF, MAX, MIN, TST, and XOR Instructions |
The following shows the DIV, DIVU, EMUL, EMULU, ITOF, MAX, MIN, MUL, TST, and XOR instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.18 | Instruction Formats of DIV, DIVU, EMUL, EMULU, ITOF, MAX, MIN, TST, and XOR Instructions |
|
|
|
|
|
|
|
|
|
DIV/DIVU/
EMUL/EMULU/ITOF/
MAX/MIN/TST/XOR
|
#simm:8
|
|
Rd
|
4
|
|
#simm:16
|
|
Rd
|
5
|
|
#simm:24
|
|
Rd
|
6
|
|
#imm:32
|
|
Rd
|
7
|
|
src,dest
|
dsp:8[Rs].memex
|
|
Rd
|
4 (memex = UB), 5 (memex UB)
|
|
dsp:16[Rs].memex
|
|
Rd
|
5 (memex = UB), 6 (memex UB)
|
In the ITOF instruction, #simm:8/16/24 and #imm:32 are not allowed for src.
(8) | FADD, FCMP, FDIV, FMUL, and FTOI Instructions |
The following shows the FADD, FCMP, FDIV, FMUL, and FTOI instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.19 | Instruction Formats of FADD, FCMP, FDIV, FMUL, and FTOI Instructions |
|
|
|
|
|
|
|
|
|
FADD/FCMP/FDIV/
FMUL/FTOI
src,dest
|
#imm:32
|
|
Rd
|
7
|
|
dsp:8[Rs].L
|
|
Rd
|
4
|
|
dsp:16[Rs].L
|
|
Rd
|
5
|
In the FTOI instruction, #imm:32 is not allowed for src.
(9) | MVTC, STNZ, and STZ Instructions |
The following shows the MVTC, STNZ, and STZ instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.20 | Instruction Formats of MVTC, STNZ, and STZ Instructions |
|
|
|
|
|
|
|
|
|
MVTC/STNZ/STZ
src,dest
|
#simm:8
|
|
Rd
|
4
|
|
#simm:16
|
|
Rd
|
5
|
|
#simm:24
|
|
Rd
|
6
|
|
#imm:32
|
|
Rd
|
7
|
The following shows the MOV instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.21 | Instruction Formats of MOV Instruction |
|
|
|
|
|
|
|
|
|
|
|
MOV(.size) src,dest
|
B/W/L
|
size
|
Rs (Rs=R0-R7)
|
|
dsp:5[Rd] (Rd=R0-R7)
|
2
|
|
B/W/L
|
L
|
dsp:5[Rs] (Rs=R0-R7)
|
|
Rd (Rd=R0-R7)
|
2
|
|
B/W/L
|
L
|
#uimm:8
|
|
dsp:5[Rd] (Rd=R0-R7)
|
3
|
|
L
|
L
|
#uimm:4
|
|
Rd
|
2
|
|
L
|
L
|
#uimm:8
|
|
Rd
|
3
|
|
L
|
L
|
#simm:8
|
|
Rd
|
3
|
|
L
|
L
|
#simm:16
|
|
Rd
|
4
|
|
L
|
L
|
#simm:24
|
|
Rd
|
5
|
|
L
|
L
|
#imm:32
|
|
Rd
|
6
|
|
B
|
B
|
#imm:8
|
|
[Rd]
|
3
|
|
W/L
|
W/L
|
#simm:8
|
|
[Rd]
|
3
|
|
W
|
W
|
#imm:16
|
|
[Rd]
|
4
|
|
L
|
L
|
#simm:16
|
|
[Rd]
|
4
|
|
L
|
L
|
#simm:24
|
|
[Rd]
|
5
|
|
L
|
L
|
#imm:32
|
|
[Rd]
|
6
|
|
B
|
B
|
#imm:8
|
|
dsp:8[Rd]
|
4
|
|
W/L
|
W/L
|
#simm:8
|
|
dsp:8[Rd]
|
4
|
|
MOV(.size) src,dest
|
W
|
W
|
#imm:16
|
|
dsp:8[Rd]
|
5
|
|
L
|
L
|
#simm:16
|
|
dsp:8[Rd]
|
5
|
|
L
|
L
|
#simm:24
|
|
dsp:8[Rd]
|
6
|
|
L
|
L
|
#imm:32
|
|
dsp:8[Rd]
|
7
|
|
B
|
B
|
#imm:8
|
|
dsp:16[Rd]
|
5
|
|
W/L
|
W/L
|
#simm:8
|
|
dsp:16[Rd]
|
5
|
|
W
|
W
|
#imm:16
|
|
dsp:16[Rd]
|
6
|
|
L
|
L
|
#simm:16
|
|
dsp:16[Rd]
|
6
|
|
L
|
L
|
#simm:24
|
|
dsp:16[Rd]
|
7
|
|
L
|
L
|
#imm:32
|
|
dsp:16[Rd]
|
8
|
|
B/W/L
|
L
|
dsp:8[Rs]
|
|
Rd
|
3
|
|
B/W/L
|
L
|
dsp:16[Rs]
|
|
Rd
|
4
|
|
B/W/L
|
size
|
Rs
|
|
dsp:8[Rd]
|
3
|
|
B/W/L
|
size
|
Rs
|
|
dsp:16[Rd]
|
4
|
|
B/W/L
|
size
|
[Rs]
|
|
dsp:8[Rd]
|
3
|
|
B/W/L
|
size
|
[Rs]
|
|
dsp:16[Rd]
|
4
|
|
B/W/L
|
size
|
dsp:8[Rs]
|
|
[Rd]
|
3
|
|
B/W/L
|
size
|
dsp:16[Rs]
|
|
[Rd]
|
4
|
|
B/W/L
|
size
|
dsp:8[Rs]
|
|
dsp:8[Rd]
|
4
|
|
B/W/L
|
size
|
dsp:8[Rs]
|
|
dsp:16[Rd]
|
5
|
|
B/W/L
|
size
|
dsp:16[Rs]
|
|
dsp:8[Rd]
|
5
|
|
B/W/L
|
size
|
dsp:16[Rs]
|
|
dsp:16[Rd]
|
6
|
The following shows the MOVU instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.22 | Instruction Formats of MOVU Instruction |
|
|
|
|
|
|
|
|
|
|
|
MOVU(.size) src,dest
|
B/W
|
L
|
dsp:5[Rs] (Rs=R0-R7)
|
|
Rd (Rd=R0-R7)
|
2
|
|
B/W
|
L
|
dsp:8[Rs]
|
|
Rd
|
3
|
|
B/W
|
L
|
dsp:16[Rs]
|
|
Rd
|
4
|
The following shows the PUSH instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.23 | Instruction Formats of PUSH Instruction |
|
|
|
|
|
|
|
|
|
PUSH src
|
dsp:8[Rs]
|
|
|
3
|
|
dsp:16[Rs]
|
|
|
4
|
The following shows the ROUND instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.24 | Instruction Formats of ROUND Instruction |
|
|
|
|
|
|
|
|
|
ROUND src,dest
|
dsp:8[Rs]
|
|
Rd
|
4
|
|
dsp:16[Rs]
|
|
Rd
|
5
|
The following shows the SCCnd instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.25 | Instruction Formats of SCCnd Instruction |
|
|
|
|
|
|
|
|
|
|
SCCnd(.size) src,dest
|
B/W/L
|
|
|
dsp:8[Rd]
|
4
|
|
B/W/L
|
|
|
dsp:16[Rd]
|
5
|
The following shows the XCHG instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.26 | Instruction Formats of XCHG Instruction |
|
|
|
|
|
|
|
|
|
|
XCHG src,dest
|
L
|
dsp:8[Rs].memex
|
|
Rd
|
4(memex = UB), 5(memex UB)
|
|
L
|
dsp:16[Rs].memex
|
|
Rd
|
5(memex = UB), 6(memex UB)
|
(16) | BCLR, BNOT, BSET, and BTST Instructions |
The following shows the BCLR, BNOT, BSET, and BTST instruction formats and operands for which the assembler selects the optimum code, in the order of selection priority.
Table 5.27 | Instruction Formats of BCLR, BNOT, BSET, and BTST Instructions |
|
|
|
|
|
|
|
|
|
|
BCLR/BNOT/BSET/BTST
src,dest
|
B
|
#imm:3
|
|
dsp:8[Rd].B
|
3
|
|
B
|
#imm:3
|
|
dsp:16[Rd].B
|
4
|
|
B
|
Rs
|
|
dsp:8[Rd].B
|
4
|
|
B
|
Rs
|
|
dsp:16[Rd].B
|
5
|