Windows/panels/dialog boxes for debugging are listed below.
Controls the program execution. Various windows, panels and dialog boxes can be opened from this window. |
|
Selects a core (PE) to be debugged and displays the core status. |
|
Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed. |
|
Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug. |
|
Displays the contents of CPU registers, and modifies register values. |
|
Displays detailed information on set events, switches the events between enabled and disabled, or deletes them. |
|
Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box. |
|
Selects files to be downloaded and sets the download conditions. |
|
Selects the one that you wish to take precedence over other projects in stand-along debugging. |
|
Specifies the number of view columns of memory values on the Memory panel. |
|
Specifies an offset value for the address display on the Memory panel. |
|
Sets the address range to print the contents of the Disassemble panel. |
|
Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20] |
Displays and modifies the detailed information on the point trace event. |
Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20] |
Displays and modifies the detailed information on the timer event. |
Detailed Settings of Performance Measurement dialog box [Full-spec emulator][E1][E20] |
Displays and modifies the detailed information on the Performance Measurement event. |
Sets the scroll range for the Memory panel/Disassemble panel. |
|
Saves the settings and other data displayed in the respective windows/panels/dialog boxes or saves upload data. |
|
Displays the functions that access variables in the form of an orthogonal table. |
|
Checks whether exclusive control is correctly performed for a certain variable and makes the settings required for checking. |
|
This panel is central to the function of the solution for pseudo-error debugging. |
|
Select Pseudo-Error dialog box [Full-spec emulator][E1][E20] |
Selects ECM pseudo-errors displayed in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]. |
Sets the breakpoints that are to be registered to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]. |
|
Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20] |
This panel is central to the function of the solution for debugging of CAN bus reception. |
RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20] |
|
Receive Channel Setting dialog box [Full-spec emulator][E1][E20] |
|
Transmit Channel Setting dialog box [Full-spec emulator][E1][E20] |
|
Transmit Frame Setting dialog box [Full-spec emulator][E1][E20] |