This dialog box is used to select files for downloading and configure download conditions (see "2.5 Download/Upload Programs").
Note that files specified as build targets in a project (main project or sub-project) are automatically registered as download targets (they can be unregistered).
This section describes the following.
On the [Download File Settings] tab of the Property panel, click the [...] button displayed by selecting the [Download files] property in the [Download] category. |
Displays a list of files to download. The names of files specified as build targets in a project (main project or sub-project) are displayed by default (they can be removed).
Files are downloaded in the order that they are displayed here.
To add a new file to be downloaded, click the [Add] button in this area, then in the [Download file property] area, specify the download conditions of the file to add.
|
Moves the selected file down one row in the list. Clicking this for the bottom file in the list has no effect. |
|
|
Adds an empty item "-" to the list, and selects it. Specify the download conditions of the file to add in the [Download file property] area. Note that this button will be disabled if 20 files have already been registered. |
|
|
Removes the selected file from the list. Note, however, that this button is disabled if the selected file is a project build target. |
By hovering the mouse cursor over a file name, the pass information of the file is pop-up displayed. |
By dragging a file name with the mouse, the display order in the list can be changed. |
This area is used to display or edit the download conditions of the file selected in the [Download file list] area.
It can also be used to specify the download conditions of new download files added via the [Add] button.
|
Directly enter from the keyboard, or specify with the Select Download File dialog box that is opened by clicking the [...] buttonNote 1 appears at right by selecting this item. |
||||
|
Specify the offset from the address at which the file's download is to start. Note that this item appears only when [File type] or [S-record file] is set to [Hex file]. |
||||
|
Specify the address at which to start the file's download. Note that this item appears only when [File type] is set to [Binary data file]. |
||||
|
Specify whether to download the object information from the specified file. Note that this item appears only when [File type] is set to [Load module file]. |
||||
|
Specify whether to download the symbol information from the specified fileNote 2. Note that this item appears only when [File type] is set to [Load module file]. |
||||
|
Select whether to generate the information for the Symbol name completion function when downloadingNote 3. Note that this item appears only when [File type] is set to [Load module file]. |
||||
|
Generates the information for the symbol name completion function. (i.e. uses the symbol name completion function.) |
||||
|
Does not generate the information for the symbol name completion function. (i.e. does not use the symbol name completion function.) |
||||
When a file specified as build target in the project is selected in the [Download file list] area, or when the program is executing, the [...] button does not appear. |
If the symbol information have not been downloaded, the source level debugging cannot be performed. |
When [Yes] is selected, the time taken for downloading and the memory usage on the host machine will increase. We recommend selecting [No] in this item if you do not intend to use the symbol name completion function. |