2.17.5 Deleting events

To delete any event you've set, select the subject event and then click the toolbar button .

When an event is specified by a combination of multiple events, each event in the detailed information can be deleted independently.

However, you cannot delete the unconditional trace event and Run-Break timer event, which are the built-in events of the debug tool.

Remark 1.

For the timer start and end events, and trace start and end events, you can also delete an event by selecting [Delete Event(s)] from the context menu displayed by right-clicking the event mark that is displayed on the Editor panel or Disassemble panel.

Remark 2.

For the software/hardware break and the trace event consisting of execution-related events, you can delete an event by clicking their event mark that is displayed on the Editor panel or Disassemble panel.

Remark 3.

To delete all of the events youve set at a time, select [Select All] on the context menu and then click the button (not including the built-in events).