This function refers to a variable value.
[Specification format]
debugger.Watch.GetValue(variableName, encode = Encoding.Default, watchOption = WatchOption.Auto)
|
[Argument(s)]
|
|
|
|
variableName
|
Specify the variable name, register name, or I/O register name/SFR register name to reference.
|
|
encode
|
Specify the encoding to use when displaying strings.
By default, the system encoding is used.
The encoding name conforms to the .NET specifications.
Examples: Encoding.utf-8, Encoding.euc-jp
|
|
watchOption
|
Specify an option.
The options that can be specified are shown below.
|
|
|
|
|
WatchOption.Auto
|
Automatically detect when displaying (default).
|
|
WatchOption.Binary
|
Display in binary format.
|
|
WatchOption.Octal
|
Display in octal format.
|
|
WatchOption.Decimal
|
Display in decimal format.
|
|
WatchOption.SignedDecimal
|
Display in signed decimal format.
|
|
WatchOption.UnsignedDecimal
|
Display in unsigned decimal format.
|
|
WatchOption.Hexdecimal
|
Display in hexadecimal format.
|
|
WatchOption.String
|
Display as a string.
|
|
WatchOption.Sizeof
|
Display the variable size in decimal format.
|
|
WatchOption.Float
|
Display in float type.
|
|
WatchOption.Double
|
Display in double type.
|
[Return value]
The displayed value is returned in the format specified by watchOption.
When watchOption is specified as "WatchOption.Auto", the format is returned to match the variable value.
However, if the return value is a double type, it is returned as a string (when watchOption is specified as "WatchOption.Double", or watchOption is specified as "WatchOption.Auto" and the return value is a double type).
[Detailed description]
- | This function displays the value of the variable specified by variableName. |
- | If encode is specified, then perform encoding using encode. |
- | If watchOption is specified, display according to watchOption. |
Caution | When a load module name or file name is specified as a variable (variableName), it needs to be enclosed in double quotation marks (" ") in some cases. See "CS+ Integrated Development Environment Users Manual: Debug Tool" for details. |
Example | When file name "C:\path\test.c" and variable "var" are specified |
Or
"\"C:\\path\\test.c\"#var"
|
[Example of use]
>>>debugger.Watch.GetValue("testVal")
128
>>>debugger.Watch.GetValue("testVal", WatchOption.Hexdecimal)
0x80
>>>debugger.Watch.GetValue("testVal", WatchOption.Binary)
0b10000000
|