|
debugger.Interrupt.SetTimer
|
This function sets the timer interrupt. [RH850 Simulator]
[Specification format]
debugger.Interrupt.SetTimer(time, timeType = TimeType.Ms, periodic = False)
|
[Argument(s)]
|
|
|
|
time
|
Specify the break time.
|
|
timeType
|
Specify the break time unit.
The units that can be specified are shown below.
|
|
|
|
|
TimeType.Min
|
Minute unit
|
|
TimeType.S
|
Second unit
|
|
TimeType.Ms
|
Millisecond unit (default)
|
|
TimeType.Us
|
Microsecond unit
|
|
TimeType.Ns
|
Nanosecond unit
|
|
periodic
|
Specify whether to call the callback every time the specified time elapses.
True: Call at every specified time interval.
False: Call one time only (default).
|
[Return value]
If the timer interrupt was set successfully: True
If there was an error when setting the timer interrupt: False
[Detailed description]
- | This function sets the timer interrupt. |
- | The calling interval of a timer interrupt depends on the simulator. |
- | Register the Python function that is processed after the specified time passes. See Hook for detail. |
[Example of use]
>>>debugger.Interrupt.ReferTimer()
None
>>>debugger.Interrupt.SetTimer(1, TimeType.S, True)
True
>>>debugger.Interrupt.ReferTimer()
1Second Periodic
|