This function sets a variable value.
[Specification format]
debugger.Watch.SetValue(variableName, value)
|
[Argument(s)]
|
|
|
|
variableName
|
Specify the variable name, register name, and I/O register name or SFR register name to set.
|
|
value
|
Specify the value to set.
|
[Return value]
If a variable value was set successfully: True
If there was an error when setting a variable value: False
[Detailed description]
- | This function sets the value specified by value in the variable, register, and I/O register or SFR register specified by variableName. |
Caution | When a load module name or file name is specified as a variable (variableName), it needs to be enclosed in double quotation marks (" ") in some cases. See "CS+ Integrated Development Environment Users Manual: Debug Tool" for details. |
Example | When file name "C:\path\test.c" and variable "var" are specified |
Or
"\"C:\\path\\test.c\"#var"
|
[Example of use]
>>>debugger.Watch.GetValue("testVal")
128
>>>debugger.Watch.GetValue("testVal", WatchOption.Hexdecimal)
0x80
>>>debugger.Watch.GetValue("testVal", WatchOption.Binary)
0b10000000
>>>debugger.Watch.SetValue("testVal", 100)
True
>>>debugger.Watch.GetValue("testVal")
100
>>>debugger.Watch.GetValue("testVal", WatchOption.Hexdecimal)
0x64
>>>debugger.Watch.GetValue("testVal", WatchOption.Binary)
0b1100100
>>>debugger.Watch.SetValue("testVal", 0x256)
True
>>>debugger.Watch.GetValue("testVal", WatchOption.Hexdecimal)
0x256
|