2.3.1 Start a project

On the tool bar, click to open the Start panel. You can click the buttons on the panel to create a new project or open an existing one.

Note that the Start panel opens automatically the first time that CS+ starts.

Figure 2.5

Start Panel