2.3.3 Add a new subproject

Select the Project node on the project tree and if you select [Add] >> [Add New Subproject...] on the context menu, the Create Project dialog box will open.

Figure 2.9

Create Project Dialog Box (When Adding a New Subproject)

 

After setting each item on the dialog box, click the [Create] button (For more on the settings for each item, see "2.3.2 Create a new project").

Remark

You can create a subproject with CC-RL as the build tool by reusing the file structure of a subproject with CA78K0R as the build tool (See "CS+ Integrated Development Environment Users Manual: Build Tool Operation" for details).

 

The project tree after adding the subproject will look like the one below.

Figure 2.10

Project Tree Panel (After Adding a Subproject)