|
r_uartfn_interrupt_receive
|
Performs processing in response to the LIN-UART reception end interrupt INTLR.
Remark | This API function is called as the interrupt process corresponding to the LIN-UART reception end interrupt INTLR. |
[Syntax]
CA78K0R Compiler
__interrupt static void r_uartfn_interrupt_receive ( void );
|
CC-RL Compiler
static void __near r_uartfn_interrupt_receive ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.