Performs processing in response to the LIN-UART reception end interrupt INTLR.
This API function is called as the callback routine of interrupt process r_uartfn_interrupt_receive corresponding to the LIN-UART reception end interrupt INTLR (performed when number of received data specified by R_UARTFn_Receive argument rx_num has been completed). |