Halts the clock supplied to the asynchronous serial interface LIN-UART (UARTF).
Remark | Calling this API function changes the asynchronous serial interface LIN-UART (UARTF) to reset status.
For this reason, writes to the control registers after this API function is called are ignored.
|
[Syntax]
void R_UARTFn_Set_PowerOff ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.