Renesas Electronics
r_dmacn_callback_transfer_end
Performs processing in response to the transfer end interrupt.
Remark
This API function is called as thecall r_dmac_dmacni_interrupt back routine.
[Syntax]
static void r_dmacn_callback_transfer_end ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]