Renesas Electronics
Below is a list of API functions output by the Code Generator for DMA controller use.
Table 3.8
API Functions: [DMA Controller]
API Function Name
Function
R_DMAC_Create
Performs initialization necessary to control the DMA controller.
R_DMAC_Create_UserInit
Performs user-defined initialization relating to the DMA controller.
r_dmac_dmacni_interrupt
Performs processing in response to the transfer end interrupt.
r_dmacn_callback_transfer_end
r_dmacn_callback_transfer_escape_end
Performs processing in response to the escape transfer end interrupt.
R_DMACn_Start
Allows starting of the DMAC controller.
R_DMACn_Stop
Prohibits starting of the DMAC controller.
R_DMACn_Set_SoftwareTrigger
Sets the software request of DMA transfer by software.
R_DMACn_Clear_SoftwareTrigger
Clears the software request of DMA transfer by software.