r_dmacn_callback_transfer_escape_end


Performs processing in response to the escape transfer end interrupt.

Remark

This API function is called as the r_dmac_dmacni_interrupt callback routine, which is generated by escape transfer end.

 

[Syntax]

static  void    r_dmacn_callback_transfer_escape_end ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.