Renesas Electronics
R_LVDn_Create_UserInit
Performs user-defined initialization relating to the voltage detection circuit.
Remark
This API function is called as the R_LVDn_Create callback routine.
[Syntax]
void R_LVDn_Create_UserInit ( void );
n is the circuit number.
[Argument(s)]
None.
[Return value]