3.2.3  
Voltage detection circuit (LVDA)
 
Below is a list of API functions output by the Code Generator for voltage detection circuit use.
| 
Table 3.3 | API Functions: [Voltage Detection Circuit] | 
|  |  | 
| 
R_LVDn_Create | 
Performs initialization necessary to control the voltage detection circuit. | 
| 
R_LVDn_Create_UserInit | 
Performs user-defined initialization relating to the voltage detection circuit. | 
| 
r_lvd_lvdn_interrupt | 
Performs processing in response to the voltage monitoring n interrupt. | 
| 
R_LVDn_Start | 
Starts voltage monitoring (when in interrupt mode, and interrupt & reset mode). | 
| 
R_LVDn_Stop | 
Ends voltage monitoring (when in interrupt mode, and interrupt & reset mode). |