Performs processing in response to the voltage monitoring n interrupt.
Remark | This API function is called to run interrupt processing for the voltage monitoring n interrupt, which is generated when the voltage detection circuit detects the voltage being dropped. |
[Syntax]
static void r_lvd_lvdn_interrupt ( void );
|
Remark | n is the circuit number. |
[Argument(s)]
None.
[Return value]
None.