|
R_RTC_Get_CalendarTimeCaptureValuen
|
Gets the captured calendar time value.
[Syntax]
void R_RTC_Get_CalendarTimeCaptureValuen ( rtc_calendarcounter_value_t * const counter_read_val );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
rtc_calendarcounter_value_t
* const counter_read_val;
|
Pointer to the area where the obtained calendar and time values.
|
Remark | The configuration of the calendar and time values rtc_calendarcounter_value_t is shown below. |
typedef struct {
uint8_t rseccnt; /* Second */
uint8_t rmincnt; /* Minute */
uint8_t rhrcnt; /* Time */
uint8_t rdaycnt; /* Date */
uint8_t rwkcnt; /* Day-of-week (0: Sunday, 6: Saturday) */
uint8_t rmoncnt; /* Month */
uint16_t ryrcnt; /* Year */
} rtc_calendarcounter_value_t;
|
[Return value]
None.