Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode).
[Syntax]
#include "r_cg_macrodriver.h"
void R_RTC_Set_BinaryAlarm ( uint32_t alarm_enable, uint32_t alarm_val );
|
[Argument(s)]
|
|
|
|
|
|
uint32_t alarm_enable;
|
Comparison flag
0x0: Comparison does not proceed
0x1: Comparison proceeds
|
|
|
uint32_t alarm_val;
|
The value of the binary counter
|
[Return value]
None.