|
R_RTC_Set_ConstPeriodInterruptOn
|
Sets the period of the periodic interrupt (PRD) and allows detection of the PRD.
[Syntax]
#include "r_cg_rtc.h"
void R_RTC_Set_ConstPeriodInterruptOn ( rtc_int_period_t period );
|
[Argument(s)]
|
|
|
|
|
|
rtc_int_period_t period;
|
Period of the periodic interrupt (PRD).
PES_2_SEC: 2 seconds
PES_1_SEC: 1 second
PES_1_2_SEC: 1/2 second
PES_1_4_SEC: 1/4 second
PES_1_8_SEC: 1/8 second
PES_1_16_SEC: 1/16 second
PES_1_32_SEC: 1/32 second
PES_1_64_SEC: 1/64 second
PES_1_128_SEC: 1/128 second
PES_1_256_SEC: 1/256 second
|
[Return value]
None.