[ RI600V4 ] tab

Outline

This tab shows the detailed information on RI600V4 to be used categorized by the following.

- Version Information

Display image





Explanation of each area

1 ) [Version Information]

The detailed information on the version of the RI600V4 are displayed.

Kernel version

Display the version of RI600V4 to be used.

Default

The version of the installed RI600V4

How to change

Changes not allowed

Install folder

Display the folder in which RI600V4 to be used is installed with the absolute path.

Default

The folder in which RI600V4 to be used is installed

How to change

Changes not allowed

Endian

Display the endian set in the project.

Display the same value as the value of the [Select endian] property of the build tool.

Default

The endian in the property of the build tool

How to change

Changes not allowed