APPENDIX A WINDOW REFERENCE
This appendix explains the window/panels that are used when the activation option for the configurator cfg600 and the table generation utility mkritbl is specified from the integrated development environment CubeSuite+.
This panel is used to display the detailed information on the Realtime OS node, system configuration file, or the like that is selected on the Project Tree panel and change the settings of the information.