powf returns a negative solution only if x < 0 and y is an odd integer. If x < 0 and y is a non-integer or if x = y = 0, powf returns a NaN and sets the macro EDOM for the global variable errno. If x = 0 and y < 0 or if an overflow occurs, powf returns +HUGE_VAL and sets the macro ERANGE for errno. If the solution vanished approaching zero, powf returns 0 and sets the macro ERANGE for errno. If the solution is a denormal number, powf sets the macro ERANGE for errno.
This function calculates the yth power of x.
#include <mathf.h> float func(void) { float ret, x, y; ret = powf(x, y); /*Returns yth power of x to ret.*/ : return(ret); } |