Arc sine
[Classification]
Mathematical library
[Syntax]
#include <mathf.h>
float asinf(float x);
[Return value]
Returns the arc sine (arcsine) of x. The returned value is in radian and in a range of -π / 2 to π / 2.
If x is not between -1 and 1, a NaN is returned, and macro EDOM is set to global variable errno.
[Description]
This function calculates the arc sine (arcsine) of x. Specify x as, -1 <= x <= 1.