Arc cosine
[Classification]
Mathematical library
[Syntax]
#include <math.h>
double acos(double x);
[Return value]
Returns the arc cosine of x. The returned value is in radian and in a range of 0 to π.
If x is not between -1 and 1, a NaN is returned, and macro EDOM is set to global variable errno.
[Description]
This function calculates the arc cosine of x. Specify x as, -1<= x <= 1.