[Initialize Routine] tab

This tab displays the initialize routine information (e.g. Start Address and Extended Information) of the RI850V4.

Figure A-25. [Initialize Routine] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the initialize routine information (e.g. Start Address and Extended Information) of the RI850V4.

This area consists of the following items.

Start Address

The start address of the initialize routine is shown.

Extended Information

The extended information of the initialize routine is shown.

Attribute

The coding language of the initialize routine is shown.

TA_HLNG

C language

TA_ASM

Assembly language



Remark Double-clicking a initialize routine information cell (e.g., Start Address or Extended Information) displays the source file of the initialize routine in the Editor panel and moves the caret to the relevant location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Start Address, Extended Information, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

Start Address, Extended Information

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Source (Start Address)

Opens the Editor panel, and displays the source code of the initialize routine.

Jump to Disassemble (Start Address)

Opens the Disassemble panel, and displays the results of disassembling the initialize routine.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).