[Interrupt Handler] tab

This tab displays the interrupt handler/CPU exception handler information (e.g. Exception Code and Start Address) of the RI850V4.

Figure A-24. [Interrupt Handler] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the interrupt handler/CPU exception handler information (e.g. Exception Code and Start Address) of the RI850V4.

This area consists of the following items.

Exception Code

An icon indicating the type of the handler and the exception code are shown in the following format.

Exception code

Start Address

The start address of the interrupt handler is shown.

Attribute

The attributes of the interrupt handler is shown.

TA_HLNG

C language

TA_ASM

Assembly language



Remark Double-clicking an interrupt handler information cell (such as Exception code or Start Address) displays the source file of the interrupt handler in the Editor panel and moves the caret to the relevant location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Exception Code, Start Address, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

Exception Code, Start Address

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Source (Start Address)

Opens the Editor panel, and displays the source code of the interrupt handler/CPU exception handler.

Jump to Disassemble (Start Address)

Opens the Disassemble panel, and displays the results of disassembling the interrupt handler/CPU exception handler.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).