2.3.5 [Simulator]

Configure the operating environment on the Property panel below when using Simulator.

Figure 2.53

Example of Property Panel [Simulator]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.5.1 [Connect Settings] tab

2.3.5.2 [Debug Tool Settings] tab

2.3.5.3 [Download File Settings] tab

2.3.5.5 [Hook Transaction Settings] tab